您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: USAF 测试卡 (131)

测试与测试目标板

Discover the different types of testing targets and their ideal applications, advantages, limitations, equations, and examples at Edmund Optics.

立即查看 添加到收藏夹

扩束镜测试

Shack-Hartmann wavefront sensors are used to test the transmitted wavefront error of laser beam expanders, predicting the real-world performance of the beam expander.

立即查看 添加到收藏夹

激光损伤阈值测试

Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.

立即查看 添加到收藏夹

爱特蒙特光学的计量技术:测量是制造的关键环节

Learn about the metrology that Edmund Optics® uses to guarantee the quality of all optical components and assemblies.

立即查看 添加到收藏夹

EO成像实验室模块2:计量和测量精度概述

Learn how to specify imaging system components.

立即查看 添加到收藏夹

现货和定制光学件制造技术

Edmund Optics is a global stock and custom optics manufacturing company with in house optical designers and on-site metrology and environmental testing.

立即查看 添加到收藏夹

解密EO成像镜头的制造过程

Imaging lens assemblies are vital components for a wide range of cutting edge applications including machine vision, biomedical instruments, factory automation, and robotics.

立即查看 添加到收藏夹

Fever Detection Using Optics

The future depends on quickly and safely detecting elevated body temperatures that may indicate the presence of contagious diseases, such as COVID-19 (novel coronavirus).

立即查看 添加到收藏夹

适用于激光应用的高反射率反射镜

The industry standard method for quantifying reflectivity does not tell the whole story

立即查看 添加到收藏夹

Optics for Antibody Detection

Optics aid in the quick and accurate serological detection of antibodies to determine if a subject has an immune response to COVID-19, or the novel coronavirus.

立即查看 添加到收藏夹

Using IR Spectroscopy for Counterfeit Drug Detection

Infrared spectroscopy is used to detect harmful chemicals in counterfeit drugs making it critical to combat the opioid crisis, in the field or the lab.

立即查看 添加到收藏夹

成像镜头的加固

Have an application in a demanding environment? Learn about the different types of ruggedization: industrial, ingress protection, and stability at Edmund Optics.

立即查看 添加到收藏夹

Danfoss:爱特蒙特光学案例研究

Monitoring and regulating air pollution is an essential step towards creating a cleaner environment.

立即查看 添加到收藏夹

EO 全球制造基地

Edmund Optics® (EO) manufactures millions of precision optical components and subassemblies every year in our 5 global manufacturing facilities.

立即查看 添加到收藏夹

分辨率和对比度对比

Learn how Edmund Optics maintains optical performance across the entire image plane through this resolution and contrast comparison using our C Series FFL lens.

立即查看 添加到收藏夹

Ruggedized Imaging Systems for Harsh Environments

The growth of automation has introduced machine vision lenses to more harsh environments involving shock, vibration, contaminants, and temperature swings.

立即查看 添加到收藏夹

LIDT 规范中的 不确定性

Laser induced damage threshold (LIDT) of optics is a statistical value influenced by defect density, the testing method, and fluctuations in the laser.

立即查看 添加到收藏夹

激光光学计量

Metrology is critical for ensuring that optical components consistently meet their desired specifications, especially in laser applications.

立即查看 添加到收藏夹

成像电子元件101:适用于机器视觉应用的相机类型和接口

Are you new to imaging or looking for a refresh on camera types? Learn about the advantages to camera types, digital interfaces, and more at Edmund Optics.

立即查看 添加到收藏夹

光束直径对激光损伤阈值的重要性

The diameter of a laser highly affects an optic’s laser induced damage (LIDT) as beam diameter directly impacts the probability of laser damage.

立即查看 添加到收藏夹

光学像差的比较

Trying to understand optical aberrations? Check out how to identify aberrations and view examples at Edmund Optics.

立即查看 添加到收藏夹

单一材料 非球面消色差透镜

Single-Material Aspheric Achromats correct chromatic aberrations with a unique geometry, leading to numerous benefits over conventional achromatic lenses.

立即查看 添加到收藏夹

何谓成像?

在成像过程中,光线通过成像镜头从物体映射到成像传感器上,以再现物体的特征和相似性,从而达到检查、分类或分析的目的。

立即查看 添加到收藏夹

尽量减小超快系统中的热透镜效应

Specialized coatings can minimize thermal lensing in ultrafast laser systems, which are particularly susceptible to detrimental thermal effects.

立即查看 添加到收藏夹

Schwarz Mirrors

Schwarz Mirrors eliminate stray light using black, engineered fused silica substrates that maintain desired characteristics while absorbing unwanted light.

立即查看 添加到收藏夹

将C接口组件与光学笼式系统搭配使用

Edmund Optics' fixed, adjustable, and kinematic mounting components can easily be integrated into optical systems.

立即查看 添加到收藏夹

高功率光学镀膜的复杂情况

Want to know more about high-power optical coatings? Find out more about the importance, fabrication, and testing at Edmund Optics.

立即查看 添加到收藏夹

同轴照明

Are you designing a system and debating whether or not to use in-line illumination? Read more about the proper time to use in-line and comparisons at Edmund Optics.

立即查看 添加到收藏夹

边缘涂黑

Have a question about Edge-Blackening? Find more information on stray light, measuring BRDF, and more at Edmund Optics.

立即查看 添加到收藏夹

高激光损伤AR镀膜

Laser optics high reflectivity mirrors meet exceptional specifications that Edmund Optics' competitors often fail to meet. Learn more at Edmund Optics.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号